Skip Navigation Links
  • New NIBCO Lead-Free* Line Now Includes Check Valves

    Check Valve_lo

    ELKHART, IND. – (June 13, 2012)  NIBCO INC. introduces the addition of check valves to its growing line of new lead-free* products. Commercial and fire protection wafer check valves in flanged, wafer and grooved end connections are now third-party certified lead free by WQA to NSF/ANSI 372. The new check valves include twin disc, spring actuation, rubber seat and bronze disc features.

    “This new offering represents an addition to our extensive line of new lead-free valves,” said Phil Liles, NIBCO senior product manager – valves and actuation. “These check valves meet the lower levels of lead content required to meet NSF/ANSI 372.”

    Check valves are recommended for commercial and fire protection services. The new check valves Figure Numbers 900-W-LF for fire protection, and 910-LF, 920-LF and 960-LF for commercial applications range in size from 2 inches to 24 inches. NIBCO® check valves are backed by the NIBCO 5-year 125 percent limited warranty.

    Founded in 1904, NIBCO INC. is a worldwide provider of flow control solutions to the residential and commercial construction, industrial, fire protection and irrigation markets. NIBCO is headquartered in Elkhart, Ind., and has 10 manufacturing plants located throughout the United States, Mexico and Poland. Visit www.nibco.com for information on the complete line of NIBCO products.


    Media Contact:
    pr@nibco.com