• NIBCO Launches Press Extended Adapters

    • Adapter group 2
    2017-02-01

    ELKHART, IND. – (February 1, 2017) NIBCO INC. proudly announces the launch of its new Press System Extended Adapters. These new adapters are longer than the standard WROT adapters and have been specifically designed to ensure they have the necessary length for a Press crimp.

     

    “NIBCO has been the expert in copper joinery since introducing the first practical copper fitting in 1927,” stated Marilyn Morgan, Senior Product Manager – Metal Fittings. “Since then, we have continuously designed and engineered products for faster, safer and more efficient installations like the NIBCO® Press System®. The extended adapters are an excellent addition to our extensive Press product line.”

     

    The new extended adapters are manufactured from globally sourced pure copper (a premium, proven, and preferred material for plumbing and mechanical applications) at our Stuarts Draft, Va. facility, and unlike the competitive product that is manufactured from brass, they feature a larger internal dimension for less restricted water flow. They have also been designed with a step feature that defines the minimum insertion depth and helps provide placement accuracy.

     

    NIBCO offers a complete Press system including fittings, valves, and tools. If you would like to learn more about the NIBCO® Press System®, comprehensive catalogs, price sheets, and brochures can be found at http://www.nibco.com/literature.

     

     

    About NIBCO INC.

    Founded in 1904, NIBCO INC. is a leading provider of valves, fittings and flow control products for commercial, industrial and institutional construction as well as residential and irrigation markets. NIBCO is headquartered in Elkhart, IN, and has 11 manufacturing plants located throughout the United States, Mexico and Poland. Visit NIBCO.com for information on the complete line of NIBCO products.

    • Adapter group 2
  • News

    • NIBCO Announces New Product Launch: Press Extended Repair Couplings

      3/21/2019 12:00:00 AM

      NIBCO Announces New Product Launch: Press Extended Repair Couplings 2019-03-21 ELKHART, Ind. — (March 20, 2019) NIBCO INC. is proud to announce the launch of our press extended repair couplings (PC601L). These new couplings are specifically designed for pipe repair in plumbing, mechanical and hydronic

    • NIBCO Announces New Tailpiece Product Launch

      3/21/2019 12:00:00 AM

      NIBCO Announces New Tailpiece Product Launch 2019-03-21 ELKHART, Ind. — (March 20, 2019) NIBCO INC. is proud to announce the launch of our new tailpiece (PC634) pipe joining component. This product is designed for use in multiple applications which include connecting to inlets or outlets for plumbing a

    • NIBCO Adds to its Line of Hydronic Heating Fittings

      1/22/2019 12:00:00 AM

      NIBCO Adds to its Line of Hydronic Heating Fittings 2019-01-22 ELKHART, Ind. — (January 22, 2018) NIBCO INC. is proud to announce that it has filled out its line of hydronic heating press-connect fittings, including two types of elbows and a fin tube stiffener. The additions include forged bronze vent