• NIBCO Introduces PERTpro™ Tubing to its Flexible Piping System Line

    • PERT Group
      PERTpro Product Grouping
    2017-03-02

    ELKHART, INDIANA – (March 2, 2017) – NIBCO INC. is proud to announce the introduction of PERTpro™ flexible tubing for potable water plumbing and barrier tubing for hydronics and radiant heating.

    A unique combination of flexibility, economy, lack of coil set, tight dimensional tolerance, and on-time delivery, makes NIBCO® PERTpro™ the plumbing professional’s first choice for potable water distribution and radiant heating.  Dimensions of the tubing are the same as PEX enabling the use of the same fittings, tools and joining devices for an interchangeable and complete PERTpro system. PERTpro for potable water is available in red, white and blue colors with sizes ranging from ¼”-1 ¼”.  

    PERTpro barrier tubing offers a distinct advantage over barrier PEX: it is more flexible.  This means installers will find it better for making the floor loops common in radiant heating.  PERTpro barrier tubing is green in color identifying it as the environmentally friendly choice for hydronics. It is available in sizes ranging from ½”-1”.

    Visit www.nibco.com/pertpro to learn more.

    About NIBCO INC.

    Founded in 1904, NIBCO INC. is a leading provider of valves, fittings and flow control products for commercial, industrial and institutional construction as well as residential and irrigation markets. NIBCO is headquartered in Elkhart, IN, and has 11 manufacturing plants located throughout the United States, Mexico and Poland. Visit NIBCO.com for information on the complete line of NIBCO products.

    # # #

    • PERT Group
  • News

    • NIBCO Introduces PERTpro™ Tubing to its Flexible Piping System Line

      3/2/2017 12:00:00 AM

      NIBCO Introduces PERTpro™ Tubing to its Flexible Piping System Line 2017-03-02 ELKHART, INDIANA – (March 2, 2017) – NIBCO INC. is proud to announce the introduction of PERTpro™ flexible tubing for potable water plumbing and barrier tubing for hydronics and radiant heating. A unique combinat

    • WROT ACR Fittings UL Recognized to 700 PSI

      2/16/2017 12:00:00 AM

       ELKHART, INDIANA – (February 16, 2017) – NIBCO INC. is proud to announce that a select assortment of WROT ACR fittings are now UL Recognized to 700 PSI. These products have been tested to the UL 207 performance requirements.

    • NIBCO Launches Press Extended Adapters

      2/1/2017 12:00:00 AM

      ELKHART, IND. – (February 1, 2017) NIBCO INC. proudly announces the launch of its new Press System Extended Adapters. These new adapters are longer than the standard WROT adapters and have been specifically designed to ensure they have the necessary length for a Press crimp.